แบรนด์ของเรา

ยินดีต้อนรับสู่เว็บไซต์ชไนเดอร์ อิเล็คทริค

ยินดีต้อนรับสู่เว็บไซต์ของเรา
		
วันนี้เราสามารถช่วยคุณได้อย่างไร?
What is the CFI2 fault on an Altivar (ATV600, ATV900 and ATV340) drive?

Article available in these languages: ตุรกี

Issue:
Customer has the CFI2 fault on an Altivar Process Drive

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980, and APM)
Altivar Machine Drive (ATV340)

Environment:
All serial numbers

Cause:
N/A

Resolution:
The CFI2 is Configuration Transfer Error Fault.
Occurs when a configuration file can not be loaded to the device, or the configuration is not compatible with the drive.

Possible Causes:
  • The was an unsuccessful or interrupted configuration file transfer.
  • The stored configuration (HMI) was loaded from an different firmware.  For example a file saved on a newer version drive can not be loaded into an older firmware version.
Remedies:
  • Check firmware
    • Firmware should be compatible on both drives
  • Load a compatible configuration.
  • Use SoMove to transfer configuration from another drive, or modify the saved SoMove configuration to match the drive being programmed.
  • Perform a factory setting
    • [Main Menu] [File Transfer] [Factory Settings]