ค้นหาคำถามที่พบบ่อย
Altivar drives, do I need a separate run command with preset speeds?
Issue:
Wondering If I need a separate run command with preset speeds, on Altivar drives
Product Line;
Altivar drives
Environment:
All
Cause:
N/A
Resolution:
Yes, a run command is needed and the preset speed is a separate logic input. Need both to be high, to run at the preset speed.
Wondering If I need a separate run command with preset speeds, on Altivar drives
Product Line;
Altivar drives
Environment:
All
Cause:
N/A
Resolution:
Yes, a run command is needed and the preset speed is a separate logic input. Need both to be high, to run at the preset speed.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ประเภท:
ดูข้อมูลเพิ่มเติม
รุ่น:
ประเภท: