Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Which Sepam firmware versions are compatible with the ACE850 module and support the IEC 61850 protocol?

Sepam and ACE850. What are the Sepam compatible with ACE850 and IEC 61550 Protocole ?

The Sepam that are compatible with ACE850 Accessory are :

(Sepam 20 can not support the ACE850 module)
Sepam 40 with Version >= V7.00 and S/N >= 09500001
Sepam 60 with Version Base >= V7.20 and Appli >= V7.10
Sepam 80 with Version >= V6.01 and Appli >= V6.02

If you require this functionality in the above firmware, please contact your local support center to obtain the latest firmware version.

IEDL3