วันนี้เราสามารถช่วยคุณได้อย่างไร?

Does Square D offer Copper electrostatic shield for isolated shielded transformers?

Issue:
Is there an isolated transformer with a Copper electrostatic shield.

Product Line:
Transformer

Environment:
Low Voltage Transformer

Resolution:
Square D does not offer Copper electrostatic shield, Aluminum shielding is provided as standard .