ค้นหาคำถามที่พบบ่อย
What is the length (in ms) of impulse in pulsed mode of output relays (O1, O2, O3) in Sepam 20?
Goals and Symptoms
What is the length (in ms) of an impulse in pulsed mode of output relays (O1, O2, O3) in Sepam 20.
Causes and Fixes
On Sepam 20, the time duration of a pulse of an output relay in pulsed mode is 14 ms, which is the duration of an internal cycle of Sepam.
It's the same on Sepam 40.
On Sepam 80 the basic duration is the same but you can adjust if needed the duration of the pulse with control logic.
AEDL3
Legacy KB System (APS) Data: RESL201041 V1.0, Originally authored by KBAdPM on 01/20/2010, Last Edited by KBAdPM on 01/20/2010
Related ranges: Sepam series 20
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: