วันนี้เราสามารถช่วยคุณได้อย่างไร?

How to configure the communication between Lexium Controller and OPC?

In the attachment file, you will find a presentation which shows an easy way to configure the communication between Lexium Controller and OPC.
LMC_OPC.zip

This example is based on the freeware:
MatrikonOPC Explorer

You can find it here:
http://www.matrikonopc.com/

Remark: Any other OPC software can be used.


Legacy KB System (APS) Data: RESL192210 V1.0, Originally authored by MaPr on 06/26/2008, Last Edited by MaPr on 06/26/2008
Related ranges: Lexium Controller