Where can I get Short Circuit Current Ratings information for the ATV12 drives?
Issue:
ATV12 Short Circuit Current Ratings information request
Product Line:
ATV12
Environment:
All serial numbers for ATV12
Cause:
N/A
Resolution:
The (SSCR) information can be located in the Annex for ATV12 Quick Start Guide .