Issue:
ATS22 soft starter on an open delta system
Product Line:
Altistarter ATS22 and 22U
Environment:
All
Cause:
Wants to use the ATS22 on an open delta system.
Resolution:
There is nothing published that says you cannot use the ATS22 soft starters on an open delta system. If the phase to phase voltages are balanced, it should be ok.