Issue:
When attempting to activate a Power Monitoring Expert license using the Floating License Manager, there is an error thrown indicating "Request includes activation IDs for a parent license and an update license that cannot be processed together in a single request"
Product Line:
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Environment:
Power Monitoring Expert Software Configuration
Cause:
This is a screen capture of the error that will be seen:
This is because the Activation IDs included in the license request contain an activation ID for the PME base license as well as for a Segment Edition (Buildings, Data Center, and HealthCare) Cross Grade license.
Resolution:
This is an example of two activation IDs that will be included in the Entitlement Certificate that can cause this error:
Activation ID: A-LN26-####-####
Description: PME-STD Base
Activation ID: A-4B8L-####-####
Description: DC Base Cross Grade
When trying to license a Segment Edition, we only require the Segment ID. In order to resolve this error, license the activation IDs again without including the PME-STD Base activation ID.
เผยแพร่สำหรับ: ชไนเดอร์ อิเล็คทริค Thailand