วันนี้เราสามารถช่วยคุณได้อย่างไร?

UP11_Whether unity pro complies with IEC62138

Question:
Whether unity pro complies with IEC62138?

Answer:
Unity Pro with M340 controller has been yet agreed as IEC62138 compliant.
Unity Pro with M580 compliance is under evaluation & is regarded to be ok soon.