วันนี้เราสามารถช่วยคุณได้อย่างไร?

Is it possible to remove the top cover on the Altivar Process Drive?

Issue:
Removing top cover on the Altivar Process Drive.

Product Line:
Altivar Process Drive

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
The top cover helps maintain the drives IP21 ratings and should only be removed during specific mounting conditions as instructed in the installation manuals.
See attachment

ชไนเดอร์ อิเล็คทริค Thailand

เอกสารแนบ
Removing the Top Cover.png [257.13 KB]