Issue:
Can I set 0-5V analog signal on VIA and VIB on the ATV212 drive?
Product Line:
Altivar Machines, Altivar 212, S-Flex
Environment:
All model numbers, all serial numbers
Cause:
Customer wanted to use 0-5V instead of 0-10V.
Resolution:
For setting up VIA using 0-5V, then follow the steps below:
F201 = 0
F202 = 0
F203 = 50% or 5V
F204 = 60 for 60Hz in US
For setting up VIB using 0-5V, then follow the steps below:
F210 = 0
F211 = 0
F212 = 50% or 5V
F213 = 60 for 60Hz in US
In addition, please make sure SW100 (voltage/current selection for analog I/O VIA and VIB) are set for U (voltage).
เผยแพร่สำหรับ: ชไนเดอร์ อิเล็คทริค Thailand