วันนี้เราสามารถช่วยคุณได้อย่างไร?

Does the LTMR Tesys-T product line have a web server and how do I access it?

Issue:
Customer wishes to connect directly to the Tesys T via their PC, using the built-in web server.

Product Line:
LTMR, LTMR with LTME expansion module, Tesys-T series product line.

Environment:
All models including a built-in Ethernet IP and/or Modbus TCP port (LTMR**E**)

Resolution:
The Ethernet and Modbus TCP versions of the LTMR product do support an embedded HMI which can be accessed using a standard web browser:

 Microsoft Internet Explorer version 8 or later
 Mozilla Firefox version 13 or later
 Google Chrome version 19 or later
Java Free Web Pages
The latest versions of web pages are developed on a technology called as Lightweight Web App (LWA).
The web pages are independent from Java backbone, works under any environment (XP, Windows 7,
Windows 8, and so on), and also on all web browsers (Microsoft Internet Explorer, Mozilla Firefox, and
Google Chrome). TeSys T new web pages works on PC without Java installation.

For full documentation on the web server pages, please refer to the attached document, beginning on page 141

ชไนเดอร์ อิเล็คทริค Thailand

เอกสารแนบ
Tesys T Ethernet manual 2017.pdf [9.67 MB]