{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Could you clarify the meaning of "PUP" in the Comtrade file of SFT2826?

PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured with pre-trig cycles that are used to view the recording before the actual disturbance. "PUP" relates to the instantanious pickup of a protection function, input, control logic or any other condition that sends a tripping order to the CB. This information is very usefull when analyzing a comtrade file because it helps find the origin of a sepam trip and system shutdown.

Re-published to revised security level: 20 June 2008 by DRM

Applies to: SFT2826

Internal PMO/PMC Support

All content © 1992-2007 Schneider Electric

AEDL3




Legacy KB System (APS) Data: RESL188980 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/21/2008
Related ranges: SFT 2826 (OPG display)

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.