Search FAQs
In Proworx 32 when I select"Controller/Read" will the complete program be transferred from PLC to PC?
Issue:: Uploading some or all of the project in the PLC.
Product Line: Prowrox 32
Answer: Yes the entire application program will be uploaded from the PLC to PC.
You also have the option to perform a Partial Upload which would allow
specific portions of the application to be transferred. (Read / Read Extended Memory)
R-6-30-17
Product Line: Prowrox 32
Answer: Yes the entire application program will be uploaded from the PLC to PC.
You also have the option to perform a Partial Upload which would allow
specific portions of the application to be transferred. (Read / Read Extended Memory)
R-6-30-17
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: