Search FAQs

How to fix problem when TSXCUSB485 or TSXCUSB232 cable is not recognized by windows 10/11?

Issue
Windows 10 doesn't recognize the connection cable TSXCUSB485 or TSXCUSB232.

Product Line
EcoStruxure Control Expert, TSXCUSB485, TSXCUSB232

Environment
TSXCUSB485, Windows 10, Windows 11

Step 1: Uninstall the Existing TSX Cable Driver

  1. Plug in the TSXCUSB485 or TSXCUSB232 cable.
  2. Open Device Manager.
  3. Expand the Serial USB folder.
  4. Right-click the TSX cable driver and select Uninstall.

Windows 11 Considerations

    • In Device Manager, the cable may appear under Ports (COM & LPT) rather than Serial USB after successful driver installation.

Step 2: Prevent Automatic Driver Installation

  1. Open Control Panel.
  2. Navigate to: System > Advanced System Settings > Hardware
  3. Select Device Installation Settings.
  4. For the option: "Do you want to automatically download manufacturers' apps and custom icons available for your devices?"
    1. Select: No
  5. Save the changes.

Windows 11 Considerations

    • Device Installation Settings can still be accessed through Control Panel, but navigation may differ from older screenshots.
 

Step 3: Uninstall Driver Manager x64

  1. Open Registry Editor.
  2. Navigate to: HKEY_LOCAL_MACHINE\Software\Microsoft\Windows\CurrentVersion\Uninstall
  3. Search for: DriverManager x64
  4. Locate the UninstallString entry.
  5. Copy the uninstall command (typically an msiexec command).
  6. Run the command from an elevated Command Prompt to remove Driver Manager x64.

Windows 11 Considerations

    • Driver Manager x64 may also appear under: Settings > Apps > Installed Apps

Step 4: Restart the Computer

  1. Unplug the TSX cable.
  2. Restart the PC.

Step 5: Verify Microsoft .NET Framework Features

  1. Open Turn Windows features on or off.
  2. Verify that Microsoft .NET Framework is enabled, including its subcategories:
  3. Enable any missing components if required.

Windows 11 Considerations

    • Ensure .NET Framework 3.5 and .NET Framework 4.8 Advanced Services are enabled, including its subcategories.

Step 6: Install the Schneider Driver

Install one of the following:

  • SchneiderModbusDriverSuite 14.12 or later or Reinstall Unity Pro / EcoStruxure Control Expert completely.

Step 7: Confirm Successful Installation

  1. Plug the TSX cable back into the computer.
  2. Open Device Manager.
  3. Verify that the cable appears under the COM Ports section.
  4. If the cable is displayed correctly and assigned a COM port, the issue has been resolved.

Windows 11 Considerations

    • In Device Manager, the cable may appear under Ports (COM & LPT) rather than Serial USB after successful driver installation.
Note: You can find the driver files inside the installation folder.


image

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Sustainability
  • New Energy Landscape
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings