Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Why software-defined automation is reshaping industrial automation

  • 23 Jul 2025
  • 4 min read
The challenges of legacy systems
The shift to open automation
The advantages of open automation
  1. Reduced Downtime and Faster Commissioning

    Schneider Electric’s EcoStruxure Automation Expert delivers up to 70% improved engineering efficiency and reduces commissioning time by as much as 60%. Software-defined automation allows for more updates without production shutdowns and supports centralized deployment across the organization.

  2. Lower Total Cost of Ownership (TCO)

    By eliminating vendor lock-in and streamlining integration, open automation dramatically lowers lifecycle costs. ABI Research notes that the cost of automation lies more in design and maintenance than hardware, and SDA simplifies these processes. 

  3. Enhanced Scalability

    SDA enables manufacturers to scale operations without being constrained by hardware decisions made at the start of a project. ABI forecasts that installed base of edge servers will increase by more than 60% by 2027, supporting the rise of SDA adoption. 

The multiplier effect of intelligence

The broader impact: building a resilient, sustainable future
The future is open and intelligent

Latest in Universal Automation

  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings