{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Video: What does a flashing E on the ATV212 or ATV21 display (External Fault on the graphic keypad) mean?

Article available in these languages: Czech, Spanish

Issue:
What does a blinking E on the ATV21 or ATV212 display mean?
What does External Fault mean on the graphic keypad?

Product Line:
Altivar 21
ATV21
Altivar 212
ATV212
S-flex enclosed ATV21/ATV212

Environment:
All

Cause:
Flashing E on the display of the ATV21 or ATV212 drive.

Resolution:
The drive is in a faulted status, initiated by one of the following:
1) CMOd is set to 0 or 2, the drive is in remote mode and the keypad STOP button is pressed.  Since the drive is looking for a stop command from a logic input or serial communications, the STOP button is assigned to function as an E-STOP. (See page 87 in the ATV212 Programming Manual and attachment)

2) A logic input is assigned as External Fault, functions 11 or 45, and that logic input fault is activated.
Check the following parameters:
F111 - Terminal F logic input assignment (default = 2; run forward)
F112 - Terminal R logic input assignment (default = 6; preset speed)
F113 - Terminal RES logic input assignment (default = 10; fault reset)

To reset the fault, either cycle power to the drive or activate a logic input that is assign as Fault Reset, functions 10 or 55.


Video uses the ATV212 drive for demonstration purposes:


Schneider Electric Global

Attachment(s)

ATV212_Installation_manual_EN_S1A53832_03.pdfATV212_Installation_manual_EN_S1A53832_03.pdf [5.67 MB]
FAQ 000070517.pngFAQ 000070517.png [49.92 KB]