Schneider Electric’s EcoStruxure™ Foresight Operation Ushers in A New Era for the Built Environment
- An industry-first, unifying energy, power and building systems into one open and scalable, intelligent platform powered by AI
- Built for performance, ready for scale—the operation platform for the built environment accelerates deployment, maximizes uptime and boosts cost and operational efficiency
Schneider Electric, a global energy technology leader, today unveils EcoStruxure™ Foresight Operation, marking a transformative leap for the built environment. For the first time, energy, power and building systems are unified into a single, AI-powered platform, giving customers unprecedented control, visibility and predictive insight. The announcement was made during Schneider Electric’s Innovation Summit North America, attended by more than 2,500 customers, policymakers, employees and industry leaders this week.
By turning foresight into a strategic advantage, the next-generation operation platform empowers businesses to operate smarter, faster and more confidently across their entire infrastructure. Not only does it dissolve decades of fragmentation by natively converging building and electrical systems, EcoStruxure™ Foresight Operation streamlines engineering workflows reducing time by up to 40%, as well as boosting operational efficiency by up to 50%.
“Like an intelligent operational assistant that never sleeps, EcoStruxure™ Foresight Operation guides teams to move faster, think smarter and drive impact where it matters most, scaling operational excellence while simplifying systems into a single intuitive interface,” said Manish Kumar, EVP Digital Energy at Schneider Electric.
One Platform. Infinite Possibilities
Through AI and built-in multi-domain applications, EcoStruxure™ Foresight Operation doesn’t just monitor and respond, it continuously learns, adapts and anticipates preventing challenges before they arise. This always-on approach is driven by the most advanced AI technologies that unify and analyze data in real-time for improved decision-making across the entire built environment to deliver:
- Next-level operational efficiency: delivered through a unified platform eliminating blindspots and simplifying control. This boosts efficiency up to 50% greater than before.
- Maximized uptime and resilience: enabled with complete built-in redundancy and AI diagnostics, all safeguarded by a robust, secure platform. Interrelated electrical and mechanical issues are resolved 90% faster.
- Future-ready scalability: supporting millions of connected points with an open architecture across multisite and global operations.
- Faster deployment: with one open, flexible platform. Pre-integrated built-in domains means it’s ready to go from day one and AI-powered engineering transforms hours or work into minutes, saving up to 50% in engineering time and 500 hours during setup of large systems.
Designed for tomorrow’s demands
Facility teams face mounting pressure - from aggressive project timelines and resource shortages to increasingly complex regulatory demands. Yet most operations still rely on siloed systems for HVAC, lighting and power distribution, leaving operators to manage disconnected systems that may overlook critical interdependencies. The consequences are costly: a voltage imbalance may go unnoticed until it damages equipment, solar energy sits idle while grid power runs chillers and peak demand charges spike due to lack of coordination between building and electrical teams.
These inefficiencies are magnified in mission-critical environments like data centers, hospitals and pharmaceutical campuses, where milliseconds matter and even a brief downtime can have major consequences. Energy waste further compounds the problem: with buildings wasting up to 40% of the energy they consume, the need for intelligent, unified control has never been more urgent. At a time when systems are becoming more complex and experienced talent becomes harder to find, facility teams need tools that simplify operations.
“EcoStruxure™ Foresight Operation unifies energy, power and building domains for supervisory and control, which means systems finally speak the same language, turning complexity into simplicity. As the operation platform for the build environment, it’s unlocking the foresight organizations need to thrive in a world that demands more from every watt, every second, every space,” added Kumar.
EcoStruxure™ Foresight Operation is built to meet these demands head-on. Designed in close collaboration with customers across industries, it reflects the current and future realities. Customers interested in participating in Beta testing can get involved in the coming months. EcoStruxure™ Foresight Operation will be more widely available to early adopter customers in Q3 2026.
###
Press contact: global.pr@se.com
Related Spokespeople
Manish KUMAR
EVP Digital EnergyManish Kumar is the Executive Vice President of Schneider Electric’s Digital Energy business, where he leads global efforts to drive transformational growth and innovation. His mission: to help customers digitize and decarbonize their operations for a more sustainable future. With nearly two decades of leadership at Schneider Electric, Manish brings a unique blend of strategic vision, technological expertise, M&A experience, and global perspective. His career spans pivotal roles in Corporate Strategy, Smart Buildings, Electrical Distribution Digitization, Data Centers, Solar Inverters, and Microgrids—each contributing to Schneider Electric’s evolution as a leader in energy management. Before joining Schneider Electric, Manish held roles as a Software Engineer and Business Consultant at Infosys, where he supported clients in the Technology, Consumer Electronics, and Insurance sectors with their digital transformations. Manish holds advanced management degrees from Harvard Business School and HEC Paris, along with a Mechanical Engineering degree from Thapar University. He has served on the Supervisory Board of Planon since 2023 and was appointed Chairman in 2025. His bold idea? Let’s shape technology to enable ordinary people to do extraordinary things and make the world a more sustainable place.Read more
Attached files
Schneider Electric’s EcoStruxure™ Foresight Operation Ushers In A New Era for the Built Environment.pdf
PDF, document17/11/2025View asset
KV Foresight Operation.jpg
JPG, photos18/11/2025View asset
Contact press
Schneider Electric Global Media Relations
global.pr@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From October 2nd, 2019, in order to secure its communication, Schneider Electric certifies its contents on Wiztrust. You can check the authenticity on the website Wiztrust.com for Corporate communications.