{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the mean time between ( MTBF ) failure for the ATS48 unit?
Issue:
What is the MTBF for the ATS48 unit?

Product Line:
Altistart 48 ATS48

Environment:
All

Cause:
Spec data

Resolution:
MTBF rates for the ATS48 were determined based on standard CNET UTE C 80-180 dated July 2000.
The rates were calculated based on 335 running days per year, 12 hours per day, or 4020 hours per year.
The rates are given at two ambient temperatures: 30C and 60C.

See attached file.

Schneider Electric Global

Attachment(s)
MTBF ATS48.pdf [4.47 KB]