Issue:
ATS48 setup to run a small motor for testing
Product Line:
ATS48
Environment:
Cause:
Resolution:
From the DRC menu set the SSt parameter to On.
Use this parameter to check the soft starter in a testing or maintenance environment, on a motor whose power is very much lower than the soft starter rating (in particular for high power soft starters).
It automatically deactivates the torque control parameter, CLP.
OFF: function inactive
On: function active
SSt returns to the OFF state as soon as the control voltage is disconnected. On the next power up, the PHF fault and the CLP parameter return to their initial configuration.
ATS48 setup to run a small motor for testing
Product Line:
ATS48
Environment:
Cause:
Resolution:
From the DRC menu set the SSt parameter to On.
Use this parameter to check the soft starter in a testing or maintenance environment, on a motor whose power is very much lower than the soft starter rating (in particular for high power soft starters).
It automatically deactivates the torque control parameter, CLP.
OFF: function inactive
On: function active
SSt returns to the OFF state as soon as the control voltage is disconnected. On the next power up, the PHF fault and the CLP parameter return to their initial configuration.
Released for:Schneider Electric Global