Resolution:
Yes.
It is a programmable analog output.
Output can be configured as 0-20 mA or 4-20 mA
*Accuracy +/- 5% of the maximum value, maximum impedance 500 ohms
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.