Issue:
Err7 will not clear off the remote HMI.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Lost communication between the main control board and the remote HMI
Resolution:
Err7 indicates that the keypad and control board are not communicating properly. INI indicates that the control board is reverting to factory settings or has invalid settings. These indications combined may indicate poor or low control voltage supply to the soft starter control board.
Check the control voltage to CL1 and CL2, should be reading between 90 to 270VAC. The ERR7 fault can occur if this voltage is low. If this is a 230VAC supply application make sure that the primary side of the control transformer supplying CL1 and CL2 is wired for the 230VAC supply and not a 460VAC supply.
Keep in mind that the supply voltage is likely to drop when the motor is started due to high starting currents.
Err7 will not clear off the remote HMI.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Lost communication between the main control board and the remote HMI
Resolution:
Err7 indicates that the keypad and control board are not communicating properly. INI indicates that the control board is reverting to factory settings or has invalid settings. These indications combined may indicate poor or low control voltage supply to the soft starter control board.
Check the control voltage to CL1 and CL2, should be reading between 90 to 270VAC. The ERR7 fault can occur if this voltage is low. If this is a 230VAC supply application make sure that the primary side of the control transformer supplying CL1 and CL2 is wired for the 230VAC supply and not a 460VAC supply.
Keep in mind that the supply voltage is likely to drop when the motor is started due to high starting currents.
Released for:Schneider Electric Global