Issue:
Hand Off Auto kit needed for an enclosed LE*D, IEC starter
Product Line:
IEC Contactors and Starters
Environment:
LE1D Instakit IEC enclosed starters
Cause:
Hand off auto is required in the application
Resolution:
LA9CA06ET is the part number for the Hand-Off-Auto (HOA) selector switch Insta-Kits. This is for field installation.
Hand Off Auto kit needed for an enclosed LE*D, IEC starter
Product Line:
IEC Contactors and Starters
Environment:
LE1D Instakit IEC enclosed starters
Cause:
Hand off auto is required in the application
Resolution:
LA9CA06ET is the part number for the Hand-Off-Auto (HOA) selector switch Insta-Kits. This is for field installation.
Released for:Schneider Electric Global