{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is included with the Class 9998 Type S contact kits?
Issue:
9998 contact kit parts

Product Line:
Type S Accessories and Components

Environment:
Contactor and Starter Replacement Part Kits

Resolution:
The 3 pole contact kit will contain - 3 moveable contacts, 6 stationery contacts and 6 stationery screws.
***Springs are not included because part of the contact carrier assembly.

NOTE - 1 pole contact kit is 1 set of NO power pole contacts
- 2 pole contact kit is 2 moveable contacts and 4 stationary contacts with screws
- 4 pole contact kit is 3 moveable contacts and 6 stationary contacts with screws plus a set of NO power pole contacts.  The 4th pole power contacts are different from the normal starter contacts.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.