{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What relay should be used to provide two wire control for the Class 8903 Type PB lighting contactor?
Issue:
Two wire control relay for the Class 8903 Type PB lighting contactor

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Lighting Contactors

Cause:
Two wire control relay needed

Resolution:
Use any 2 pole relay with a Normally Open and Normally Closed contact, such as
CA2SK11**
8501XO11V**

Complete the part number by adding the appropriate voltage code.  i.e 8501XO11V02 for 120VAC, or CA2SK11G7 for 120VAC.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.