{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are the 9001K51 and 9001K52 Closing Plates Metal or Plastic?
Issue:
Clarifying is the closing plates are metal or plastic

Product Line:
9001 30mm

Environment:
North American Products

Resolution:
Both 9001K51 and 9001K52 are plastic.  They do come with a metal ring nut that secures the closing plate to the back of the enclosure.
Meets UL and Nema 1, 2, 3, 4, 4x, 6, 12, and 13.

Schneider Electric Global