Issue :
ATS48 protective covers for power terminals
Product Line :
Altistart Soft start
Environment :
ATS48
Cause :
Finger protection
Resolution :
Covers are only available for the larger frame sizes of the Altistart 48.
LA9F702 - cover for ATS48C14Y and ATS48C17Y
LA9F703 - cover for ATS48C21Y, ATS48C25Y, ATS48C32Y
*Each part number has a set of 6 terminal covers.
ATS48 protective covers for power terminals
Product Line :
Altistart Soft start
Environment :
ATS48
Cause :
Finger protection
Resolution :
Covers are only available for the larger frame sizes of the Altistart 48.
LA9F702 - cover for ATS48C14Y and ATS48C17Y
LA9F703 - cover for ATS48C21Y, ATS48C25Y, ATS48C32Y
*Each part number has a set of 6 terminal covers.
Released for: Schneider Electric Global