Issue:
Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?
Product Line:
ATV61 ATV71
Environment:
All
Cause:
Remote keypad in direct sunlight
Resolution:
No. The display cover is not UV protected. The display will not function properly if exposed to direct sunlight over time.
Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?
Product Line:
ATV61 ATV71
Environment:
All
Cause:
Remote keypad in direct sunlight
Resolution:
No. The display cover is not UV protected. The display will not function properly if exposed to direct sunlight over time.
Released for:Schneider Electric Global