Issue:
Mod F07 Hand-Off-Auto-Comm selector on the M-Flex part number request
Product Line:
ATV61 ATV71 M-Flex Model 6 MCC
Environment:
All
Cause:
Wiring
Resolution:
The Hand-Off-Auto-Comm selector is made up of the following:
KAXZ1M12 Operator Handle
9003K2H0285USX Contact Block
65170-170-41 A-O-H Legend Plate
31164-098-01 COMM Label
ZBZ32 LEGEND PLATE HOLDER
Released for: Schneider Electric Global