Issue:
Part numbers for the optional fan kit for the Altistart 22
Product Line:
ATS22
Environment:
All serial numbers for ATS22
Cause:
N/A
Resolution:
The ATS22 'S6" version utilizes 230V fans.
The ATS22 'S6U" version utilizes 120V fans.
ATS22D17..., D32, and D47 = VW3G22400 (230V) or VW3G22U400 (120V)
ATS22D62..., D75, and D88 = VW3G22401 (230V) or VW3G22U401 (120V)
ATS22C11..., C14, and C17 = VW3G22402 (230V or VW3G22U402 (120V)
This is an optional external fan that mounts to the back of the ATS22 and has a plug that attaches to the bottom of the ATS22.

See the ATS22 User Manual starting on page 20 for more details.
Part numbers for the optional fan kit for the Altistart 22
Product Line:
ATS22
Environment:
All serial numbers for ATS22
Cause:
N/A
Resolution:
The ATS22 'S6" version utilizes 230V fans.
The ATS22 'S6U" version utilizes 120V fans.
ATS22D17..., D32, and D47 = VW3G22400 (230V) or VW3G22U400 (120V)
ATS22D62..., D75, and D88 = VW3G22401 (230V) or VW3G22U401 (120V)
ATS22C11..., C14, and C17 = VW3G22402 (230V or VW3G22U402 (120V)
This is an optional external fan that mounts to the back of the ATS22 and has a plug that attaches to the bottom of the ATS22.
See the ATS22 User Manual starting on page 20 for more details.
Released for:Schneider Electric Global