{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How is the motor power scaled on an ATV61 / ATV71 analog output?
Issue:
Scaling of motor power on ATV61 / ATV71 AO1.

Product Line:
ATV61

Environment:
Analog output

Cause:
n/a

Resolution:
It is scaled from 0 to 2.5 times the Rated Motor Power (nPr), as set in the Simply Start or Motor control menus.

Schneider Electric Global