{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What class overload protection does the ATV312 drive provide?

Article available in these languages: Spanish

Issue:
ATV312 overload protection class

Product Line:
Altivar 312

Environment:
Overload protection

Cause:
n/a

Resolution:
The drive provides class 10 overload protection.
You can set this overload parameter in the SEt menu under ITH, which is based on the motor's FLA setting stamped on the motor name plate.
There is additional information in the ATV312 Programming manual.