Issue:
Altivar 312 auto restart configuration
Product Line:
ATV312
Environment:
Power outage
Cause:
n/a
Resolution:
Yes it can. If the drive is set for 2 wire control, in the IO menu, set tCC-2C and tCt-LEL (LI1- Run Forward). Go to FLT menu: Set Atr to yes. The same logic will apply to the run reverse command (LI2).
Altivar 312 auto restart configuration
Product Line:
ATV312
Environment:
Power outage
Cause:
n/a
Resolution:
Yes it can. If the drive is set for 2 wire control, in the IO menu, set tCC-2C and tCt-LEL (LI1- Run Forward). Go to FLT menu: Set Atr to yes. The same logic will apply to the run reverse command (LI2).
Released for:Schneider Electric Global