{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the pinouts for the Output Relay on the Environmental Monitoring Unit (AP9319) and the Environmental Management System (AP9320)?


Below are the pinouts:


Pin #

Description

1

No Connection

2, 3

Normally Closed (NC) Contact

4, 5

Common

6, 7

Normally Open (NO) Contact (recommended connection)

8

No Connection


Relay ratings: 1A, 30V AC/DC



Since the user interface allows for either 'normally open' or 'normally closed,' APC recommends using only the normally open contacts and configuring the 'normal' state in the user interface.



Schneider Electric Global

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: