Issue
Which UPS models are compatible with AP9622?
Where are the UPS bit registers for my Building Management Integration Card (AP9622)?
Product Line
- UPS Device Management
- AP9622 - RS-232 Modbus/JBUS Building Management Integration SmartSlot Card
Environment
- All serial numbers
- AP9622 applications
Cause
This article provides general reference material and compatibility information.
Resolution
The AP9622 supports the following UPS series:
- Smart-UPS (SU, SUA, SUM)
- Smart-UPS RT (SURT, SURTA),
- Matrix
- Symmetra (single and three phase)
- Smart-UPS VT/Galaxy 3500
- Silcon
- AIS
Bit map registers are available on the APC website under the Documentation tab: http://www.apc.com/shop/no/en/products/Modbus-Jbus-Interface-Card/P-AP9622
Released for:Schneider Electric Global