{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Network Management Card - Single Phase Symmetra SNMP Trap #77 details


Issue

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

Product Line

  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
  • UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH


Environment
  • All serial numbers
  • All firmware versions
  • SNMPv1 or v3 traps


Cause

SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type.


Resolution

Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.

Schneider Electric Global

Attachment(s)
trap77 subtraps (SY).xls [17.5 KB]