Issue:
What is the difference between the leak sensors AP9325 and AP9326?
Product line:
All InRow Units
Environment:
Data Center Cooling
Cause:
Resolution:
There are 3 main differences:
What is the difference between the leak sensors AP9325 and AP9326?
Product line:
All InRow Units
Environment:
Data Center Cooling
Cause:
Resolution:
There are 3 main differences:
- AP9325 is used for the 300mm Gen1 InRow RC , InRow SC, InRow RD, and Environment & Monitoring Systems, whereas the AP9326 is just for the Gen1 600mm InRow RP, RD, and RC
- The AP9326 is the extension cable of AP9325.
- The connection for AP9325 is RJ45, whereas the AP9326 connection is a 2 prong Molex connector. Please see below:
AP9326 | ||
600mm InRow CW | 600mm InRow DX | |
AP9325 | ||
Released for:Schneider Electric Global