{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
UPS Performs Continuous Self Tests for One Hour Before Its Scheduled Time

Issue

A UPS performs continuous self-tests for an hour before it is actually scheduled to perform one.


Product Line

Back-UPS
Smart-UPS
Smart-UPS Online/Smart-UPS RT
Symmetra Power Array
Symmetra RM
Symmetra LX


Environment

PowerChute Plus running on Netware 5 SP 3


Cause

Powerchute Plus 4.3.3 is configured to run a scheduled self test on a Netware 5 SP 3 server. However, the self test begins an hour before the scheduled time and runs continuously for that hour. This issue would only occur on Netware 5 SP 3 servers and only affected those living in states that do not observe Daylight Savings Time, such as Indiana and Arizona. Novell released SP 4 and in their list of "file fixes" it states SP 4" fixed daylight savings time calculations to function properly for time zones where there is no daylight saving and for time zones in the Southern Hemisphere".


Resolution

Installing SP 4 solves the scheduled self test issue.


Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.