{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are Symmetra LX Intelligence Modules Universal?


Yes.  There are no country or region specific versions of the SYMIM5.  It is universal and can be used in both split-phase (208/240V) Symmetra LX models as well as 3:1 / 1:1 (220/230/240V or 380/400/415V) Symmetra LX models.