{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Symmetra RM 6kVA Module Replacement Procedure

Article available in these languages: Spanish

Issue
I need to install or replace a module in my Symmetra RM 6kVA UPS system.  How do I do this?

Product Line
Symmetra RM 6kVA

Environment
All Serial Numbers

Cause
Symmetra UPS are designed with modularity so that modules can be added or replaced as needed.  This document contains video to aid the user in performing the installation of a new module or replacement of an existing module.

Resolution
The following videos detail the process of replacing the Intelligence, Battery, and Power Modules in the Symmetra RM 6kVA UPS.





Schneider Electric Global