Where are the Model and Serial numbers on the NetShelter SX, SV or VX?
Published date:
22 January 2019
Issue: Customer cannot find the serial number of the NetShelter cabinet.
Product Line: NetShelter
Environment:
All versions and serial ranges.
Cause: Need to locate the serial number.
Resolution:
The serial number and model number are located on a label inside the rear doors on the top of the frame. Simply open the rear doors and look up.
See attached file for photos.