{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What's the difference between shipping load, dynamic load and static load? Which standards are used to certify these ratings?
Issue:
Shipping, moving and loading cabinets requires the installer to know the difference between shipping load, dynamic load and static load ratings.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Installers and designers need to make sure the load capacity of the cabinet is not exceeded during installation, travel or operation.

Resolution:

Please see attachment for load ratings, definitions and standards.

Schneider Electric Global

Attachment(s)
20120330 NetShelter SX Load Rating Information Rev 7.pdf [219.69 KB]