{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How is an ATV212 or ATV21 reset to factory defaults?

Article available in these languages: Finnish

Issue:
ATV212 or ATV21 reset factory defaults.

Product Line:
ATV212, ATV21, S-Flex

Environment:
All part numbers

Cause:
Change in programming or application that requires the drive to be reset to factory default settings.

Resolution:
Set tYP = 3 to return to factory settings (remember to press and hold enter for 2 seconds).
Then set  tYP = 2 to configure for 60Hz.
Proceed with any further programming from here.

ATV212 Typ parameter

Consult the ATV212 Programming Manual or ATV21 Programming Manual for additional details: