{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there a way to get more torque out of the motor when running at lower speeds with an ATV312 drive?
Issue:
How to increase the torque out of a motor when running at lower speeds with an ATV312 drive

Product Line:
ATV312

Environment:
All

Cause:
More torque

Resolution:
First, verify that the motor data is correct in the drC menu.  Then set UFt to L.  In the SEt menu, increase UFr to provide higher torque output.