{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV312 be powered by an external 24V only?
Issue:
Powering the ATV312 by an external 24Vdc only

Product Line:
Altivar 312

Environment:
All

Cause:
Installation/programming

Resolution:
No, this drive must have line voltage applied. The voltage must be within -15% to +10% of the rated line voltage.

Schneider Electric Global