Issue:
Can the ATV312 be powered up with 120 Vac single phase for programming only?
Product Line:
Altivar 312
Environment:
All
Cause:
Need to power up the electronics of the drive for programming
Resolution:
If the ATV312 is rated for 230Vac input, you may be able to program with 120V supply power. For the 480V and 575V rated drives, 120VAC is too low for the drive to power up the control portion.
The Mulitloader is an option for programming the ATV312 without line power.
Can the ATV312 be powered up with 120 Vac single phase for programming only?
Product Line:
Altivar 312
Environment:
All
Cause:
Need to power up the electronics of the drive for programming
Resolution:
If the ATV312 is rated for 230Vac input, you may be able to program with 120V supply power. For the 480V and 575V rated drives, 120VAC is too low for the drive to power up the control portion.
The Mulitloader is an option for programming the ATV312 without line power.
Released for:Schneider Electric Global