Issue:
NST on the AC Drives
Resolution:
NSt = Drive state for freewheel stop.
Troubleshooting tips:
1. Check menu 1.7 application function, stop configuration, and freewheel stop assignment. If it is set to a logic input, then that input must be ON before the drive can run.
2. Pushing the STOP key on the HMI will trigger NST if your run command is coming from the terminal inputs. Cycle the run command to clear it.
3. If a run command is present when power is applied to the drive and tCt (2 wire type) is not set to LEL (level), NST will be triggered.
4. If the drive is being controlled over a communication network, must give the drive a run command through come, or will show a nst.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global