{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How are preset speeds configured on Altivar 212 Drives?

Issue:
Preset speeds configured on Altivar 212 Drives.

Product Line:
Altivar 212 ATV212

Environment:
All ATV212 models

Cause:
Drive is to run at 2 different specific speeds.

Resolution:
The slower speed is assigned to LL and a logic input activates the higher speed which is assigned to Sr1.
For example, logic input R is assigned F112 = 6.  When R is low, the drive runs at speed LL.  When R is high, the drive runs at speed Sr1.

Note that the Preset Speed control feature is only active when the drive is in logic input control, CMOd=0, and in Remote mode.

Schneider Electric Global