{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How is the DC injection braking setup on the ATV212 drives?
Issue:
DC injection braking setup on the ATV212 drives.

Product Line:
ATV212

Environment:
DC Injection braking

Cause:
N/A

Resolution:
Program the following:
F250 =  DC braking starting frequency, set to a value > 0
F251 =  DC braking current  level
F252 =  DC braking time

Caution:  Prolonged periods of DC injection can damage the motor.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: